Load From Data Log

This feature applies in Dynamic discharge and Profiler discharge operations.

  • Data log files (*.dlg) can be loaded from the Advanced Power control and Analysis application.

  • The data log file must contain only one trace, which is the “Current” trace.

  • If no file is loaded, or the file is unsupported, the Start button will be disabled.